Skip to main content

Please Select Your Country/Language Preferences

Print
Elexant 5010i-LIM

nVent Extends its Range of nVent RAYCHEM Elexant Connected Solutions with a New Heat Trace Controller

LONDON – May 25, 2023 – nVent Electric plc (NYSE:NVT) (“nVent”), a global leader in electrical connection and protection solutions, today announced the introduction of the nVent RAYCHEM Elexant 5010i heat trace controller to the EMEAI and APAC regions. Just as its predecessor, the nVent RAYCHEM NGC-20 controller, the Elexant 5010i controller offers the same pipe freeze protection and process temperature maintenance capabilities, but now for more extreme environments. It is also faster and offers a higher degree of accuracy and data security, with full connectivity.

The Elexant 5010i controller builds upon the legacy of the nVent RAYCHEM NGC-20 controller, which has a large installed base and has been available for more than 15 years. The new Elexant 5010i controller offers additional capabilities to extend the lifespan of critical systems, reducing waste and lowering total installed cost.

Compared to its predecessor, the Elexant 5010i controller has a wider ambient temperature range from -50°C to +60°C and comes with a faster processor, more memory, a larger Bluetooth® range and a digital SIL2 safety limiter. Its refined accuracy of measurement allows for controlling very short instrumentation lines. Furthermore, the password-protected nVent Elexant App for AndroidTM devices ensures a safe and secure configuration.

The Elexant 5010i controller shares some features with the NGC-20. The Elexant 5010i controller includes an automatic self-test function for the entire heat trace circuit. It can be centrally monitored to allow data-analysis and alarm management. Also it has the ability to connect to the client’s central process control system.

“At nVent, we are focused on delivering high value and differentiated solutions for our customers,” said Robert Kuipers, nVent product manager. “The launch of the nVent RAYCHEM Elexant 5010i controller shows our ongoing commitment to create solutions that address the safety, energy efficiency and reliability requirements of our customers today and tomorrow.”

Industry 4.0 and the Internet of Things are driven by automation and data exchange, in which interactive system communications play a vitally important role. nVents Elexant heat trace controllers are designed to collect and integrate all data into a data network, while providing customers with intuitive user interfaces and full visibility of their assets. This allows them to use data-driven insights to make more informed decisions and protect what matters most to them. As a result, operators can achieve a lower cost of ownership and improve reliability, making operations in the field easier and more productive than ever before.

About nVent

nVent is a leading global provider of electrical connection and protection solutions. We believe our inventive electrical solutions enable safer systems and ensure a more secure world. We design, manufacture, market, install and service high performance products and solutions that connect and protect some of the world's most sensitive equipment, buildings and critical processes. We offer a comprehensive range of enclosures, electrical connections and fastening and thermal management solutions across industry-leading brands that are recognized globally for quality, reliability and innovation. Our principal office is in London, United Kingdom and our management office in the United States is in Minneapolis, Minnesota. Our robust portfolio of leading electrical product brands dates back more than 100 years and includes nVent CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF and TRACER.

nVent, CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF and TRACER are trademarks owned or licensed by nVent Services GmbH or its affiliates. Android is a trademark of Google LLC. The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc.

 

Media Contact

Koen Verleyen - Marketing Manager EMEAI
[email protected]
+ +32 478 904219

Powered by Translations.com GlobalLink OneLink SoftwarePowered By OneLink