Passer au contenu principal

Sélectionnez vos préférences de pays/langue

Liquid Cooling at Scale for AI

Liquid cooling is vital for scaling AI as it effectively manages the heat produced by high-performance computing systems. This approach improves reliability, lowers energy usage, and accommodates the heavy computational requirements of AI tasks.

 

Efficient Liquid Cooling For High-Performance Computing

 

Les solutions de refroidissement liquide peuvent offrir une efficacité de refroidissement notablement supérieure à celle des traditionnelles méthodes de refroidissement par air. 

Nos solutions hybrides liquide-air aident les clients à préparer les datacenters à intégrer la technologie de nouvelle génération sans devoir refonder totalement l’architecture des datacenters.

 


 

Industry Leaders Collaborate to Advance High Performance Computing

nVent is proud to collaborate with industry experts to develop innovative technical designs aimed at addressing the most challenging high-density compute cooling issues. With over 15 years of experience in liquid cooling, nVent’s deep technical application experience and global presence enables creating efficient solutions that ensure optimal performance and reliability for advanced computing environments for our partners.


 

Liquid Cooling Solutions for GB200 and Beyond

02 DNS pouce actualités2

The Coolant Distribution Units(CDU) is the heart of the liquid cooling system, pumping the fluid at the desired temperature directly to the chips or servers.

02 DNS pouce actualités

The nVent Liquid-to-Air LTA Sidecar Heat Rejection Unit (HRU) is an integrated system that supports up to two racks of liquid-cooled IT equipment without a Facility Water System (FWS).

02 DNS pouce actualités3

Rear Door Heat Exchanger (RDHX) offer resilient operations with tool-less, hot-swappable components. The RDHX PRO upgrades data centers for high-density racks up to 78 kW, enhancing energy efficiency and space utilization.


 

INFORMATIONS

À l'approche de 2025, de nombreuses nouvelles technologies de l'information et des puces sont conçues en tenant compte du refroidissement par liquide.

Les centres de données qui ne déploient qu'un système de refroidissement par air risquent d'avoir du mal à répondre aux demandes de leurs clients à l'avenir, qui recherchent des performances accrues et des équipements informatiques de nouvelle génération. 

TrendForce’s recent report states that the launch of NVIDIA’s Blackwell platform is set to drive the adoption of liquid cooling solutions from around 10% in 2024 to over 20% in 2025.  

Many data center managers and IT professionals are turning to liquid cooling. Liquid cooling can help data centers increase capacity while maintaining efficient space and energy use. These systems can provide an effective solution for achieving the required temperature parameters of next-gen chips and reducing the energy consumption of cooling systems. 

 Unité de distribution de réfrigérant RackChiller CDU800

liquid cooling page images_02 Why Liquid Cooling.webp

 

INFORMATIONS

Que faut-il faire pour passer au refroidissement liquide ?

Constant advancements in technology and connectivity are driving new applications and an increased need to safeguard the world’s data and networks. Content streaming, online banking, cloud computing, edge computing, artificial intelligence. These are just a few examples of applications driving data demand around the world.  

Avec l'augmentation de la demande d'internet et de services cloud, les centres de données doivent augmenter leur capacité de manière exponentielle. Dans de nombreux cas, ils doivent le faire sans augmenter considérablement l'espace physique qu'ils occupent. Electrification is also driving next-generation technologies that outpace the ability of traditional data infrastructure—especially in the area of cooling. The time to consider liquid cooling is now.


 

INFORMATIONS

Trois technologies clés pour le centre de données refroidi par liquide

L'accélération de l'IA et du traitement de données haute performance modifie le paysage de l'industrie du refroidissement des centres de données. Les technologies de nouvelle génération, dont les GPU NVIDIA, nécessitent un refroidissement liquide. This technology is here to stay and expanding every year; data center managers need to think about how, not if, they will bring liquid cooling capabilities into their data centers.  

Liquid cooling uses chilled water instead of air to capture and transport heat away from chips. It can offer better performance while saving energy and helping data centers operate more sustainably. 

Liquid provides a much greater heat transfer capacity than air, which helps increase power usage effectiveness (PUE), reducing energy costs and contributing to environmental sustainability.

liquid cooling page images_06 Explosive AI Growth.webp

liquid cooling page images_04 Optimized Data Center.webp

 

 

INFORMATIONS

Optimized Data Center Solutions for a Sustainable Future

nVent recognized as top Data Center Solutions Provider

 


 

INFORMATIONS

Pourquoi les opérateurs de datacenters devraient-ils passer au refroidissement liquide ?

Les planificateurs d'installations de datacenters, les ingénieurs et les architectes thermiques sont responsables de la mise en place des services Internet et cloud à mission capitale dont nous dépendons tous. Cette infrastructure capitale nous permet de profiter des avantages des technologies en plein essor qui modifient notre façon de travailler, de faire des achats et d'interagir les uns avec les autres dans un monde électrifié.  

Les progrès constants de la technologie et de la connectivité génèrent de nouvelles applications, ainsi qu’un besoin accru de protéger les données et les réseaux du monde entier. Il est essentiel de garantir un flux continu d'informations. Dans le même temps, en raison de l'augmentation des coûts énergétiques et du besoin de réduire l'empreinte carbone, l'efficacité énergétique est plus importante que jamais. Avec l'augmentation de la demande de données, il est essentiel que les gestionnaires de datacenters puissent mettre en place des équipements à haute puissance qui répondent aux besoins en constante évolution des clients, tout en minimisant la consommation d'énergie.  

liquid cooling page images_05 Liquid Cooling.webp

DNS Cooling Brochure Mock-up.webp

 

 

RESSOURCES

Gestion thermique des datacenters

Notre gamme de produits complète comprend des solutions adaptables, modulaires et évolutives pour les applications de réseau, de centre de données et de communications.


 

PRODUCT HIGHLIGHT

High Power Density iPDUs

nVent Enlogic PDUs are distinguished by their comprehensive feature set, global manufacturing capabilities, and extensive customization options. We prioritize exceptional post-sale services and provide direct access to our engineering team, fostering collaboration with end users and integrators. 

By working closely with data center managers, we ensure our solutions meet their specific needs, optimizing power distribution and management in complex environments.

ENLOGIC Trio colors.webp

Nous sommes à votre service. 

Besoin d’informations complémentaires ? Contactez-nous pour en savoir plus sur nos applications en matière de réseaux, de centres de données et de communications. Un de nos représentants vous contactera dans les plus brefs délais.

DNS contact.webp

Powered by Translations.com GlobalLink Web SoftwarePowered by GlobalLink Web