Why Type MI is Specifically UL2196 Approved Fire-Rated Cable For Use in Hospitals
While designing commercial buildings, such as healthcare facilities, it is easy to overlook critical aspects of code. What is unique about healthcare facilities is the need to ensure that occupants
Case Study: Urban Commercial Building Retrofit – Electrification Upgrade
When a retrofit project came up requiring the installation of a fire-rated solution that could also deliver a significant increase in ampacity without consuming extra space, it was no surprise
Protecting Critical Building Circuits From Fire – Codes, Standards And Why Systems Matter
Fire safety codes and standards in the United States and Canada date back to the nineteenth-century development of automatic sprinklers. In 1897, the NFPA published the world’s first National Electrical
There are plenty of buildings that use concrete construction methods as a way to protect wiring to critical circuits. This process of encasing standard building wires supplying power to critical
Beyond UL 2196 – Important Safety Findings for Fire Rated Cable Systems
If your building contains a fire rated wiring system providing power to critical life safety applications (fire pumps, emergency lighting and smoke evacuation, etc.), the standard you need to follow
Why Fire-Rating Wiring is Crucial in Healthcare Buildings
When an emergency happens in a medical building, the need for quick response and protection of critical circuits is dire. In fact, medical professionals have a protocol to quickly respond
When it comes to fire rated wiring, there is a lot of discussion around safety standards and codes that building professionals need to follow. Let’s discover who is behind these
When it comes to the protection of critical electrical systems in buildings, there are a few different options to meet industry codes and standards. One of those options is copper-clad
3 Reasons Fire Chiefs Endorse 2 Hour Fire-Rated Cable
For Fire Chiefs, safety is paramount in an emergency situation. In fact, Fire Chiefs rely on a series on NPFA codes to provide essential benchmarks for a safe response to